Builder of world’s largest offshore crane vessel chooses Emerson’s valve remote control solution

HeeremaSleipnir

SSCV Sleipnir. Images courtesy of Heerema Marine Contractors. 
High resolution image - front

 // 

High resolution image - back

Valve, actuator and control package helps to ensure safe and reliable ballast operations aboard record-breaking semi-submersible

SINGAPORE (January 5, 2017) – Heerema Marine Contractors has chosen Emerson Automation Solutions to provide a valve remote control (VRC) system for the world’s largest semi-submersible offshore crane vessel, SSCV Sleipnir, currently under construction at Sembcorp Marine’s shipyard in Singapore.

The 220 meter-long vessel is designed for the installation and removal of large offshore structures, such as oil and gas platforms, subsea production facilities, foundations, moorings, and deep water floating structures. Each of the ship’s two revolving cranes is capable of lifting up to 10,000 metric tons. The critical task of stabilizing Sleipnir during lifting operations will be carried out by the ship’s ballast control system, which transfers water between onboard tanks to counter-balance the weight of shifting loads.

Not only must the ballast control system operate reliably in demanding marine conditions, but it must do so on an extraordinary scale. To address these unique challenges, Emerson’s experts worked closely with the stakeholders to design a custom, fully-redundant DamcosTM VRC solution for the ship’s fluid management and ballast systems that includes a total of 847 valves, actuators, local power units (LPUs), and eight interface cabinets connected by a P-NET communication bus.

Emerson’s Damcos LPUs are rated at IP68, meaning that they are able to operate while submerged at a depth of three bar (30 meters) for at least 24 hours. The LPUs are mounted directly on the actuators and connected to the P-NET network, saving the shipyard installation man-hours by eliminating hydraulic tubing and greatly improving reliability with their short circuit-tolerant design. This configuration allows any LPU to fail entirely without affecting the other units in the loop.

“A groundbreaking project like this called for us to partner with automation experts who could provide a VRC solution that minimized cost, weight, size, and energy use while ensuring years of safe operation in some of the toughest situations imaginable,” said Leo Stobbe, commissioning manager for Sleipnir at Heerema. “Across the board, we are confident that Emerson has delivered.”

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.