Enhanced Reservoir Software Offers More Robust Risk Analysis and Reserves Estimates

1805-roxar-tempest-8.2_edited

Roxar Tempest 8.2 reservoir management software provides risk mitigation, decision support and workflow integration from geosciences to production.
High Resolution Image


Roxar Tempest™ 8.2 comes with Big Loop™ extensions and greater third-party integration, taking reservoir engineers beyond traditional flow simulation capabilities and delivering greater project certainty through improved risk analysis.

STAVANGER, NORWAY (May 8, 2018) – Emerson has launched Roxar Tempest™ 8.2 – the latest version of its reservoir management software, bringing advanced uncertainty analysis tools and increased support to the Big Loop™ workflow and robust risk analysis and reserves estimates across the seismic-to-simulation workflow. The announcement also further strengthens Emerson’s end-to-end Exploration and Production (E&P) software portfolio, helping operators achieve top-quartile performance and greater project certainty on investment and operational goals within new and established reservoirs.

Enhancements to the Big Loop workflow within Tempest ENABLE, Emerson’s uncertainty management and history matching module, centre on greater connectivity to other IT ecosystems, leading to the closer integration of geology and engineering, simpler workflow setup and improved risk and uncertainty analysis. To this end, the system now supports the Nexus* and CMG simulators, several cluster queueing systems, such as LSF, PBS and UGE, and it is easier to connect other third-party and internal applications into the workflow. Post processing and analysis of the Big Loop ensembles is also now fully integrated.

Tempest MORE 8.2, the reservoir simulator, can now handle gas liquid recovery plants, enabling the calculating of liquid petroleum gas (LPG) and natural gas liquids (NGLs) production. In addition, the modelling of the physical processes for near well bore flow and for multiple simultaneous fluid types is enhanced. All results can be visualised in the Tempest VIEW module.

“What sets Roxar Tempest apart is our commitment to go beyond traditional flow simulation and generate an automated workflow that expands upstream into geological modelling and downstream into production management and economics for a more consistent reservoir understanding and greater project certainty,” said Kjetil Fagervik, vice president of product development of Roxar software at Emerson Automation Solutions. “With Tempest 8.2, we are one step closer to achieving this – embedding our Big Loop workflow further into our reservoir management suite, expanding MORE’s capabilities, and providing the very best in risk mitigation, decision support, workflow integration and reserves estimations from geosciences right through to production.”

The Big Loop workflow is the cornerstone of Emerson’s reservoir characterisation and modelling process, tightly integrating the static and dynamic domains and propagating uncertainties from seismic characterisation through to geological modelling and simulation. Reservoir uncertainties are captured and varied as input parameters, creating an ensemble of realistic reservoir models that all feed into the reservoir simulator. This leads to a better understanding of the reservoir geometry, more robust reserves estimations, and better-informed decisions for future field development scenarios.

Users of Tempest 8.2 will also enjoy additional post processing capabilities through Tempest VIEW. These include full support for the latest CMG simulator output, direct creation of PowerPoint presentations and improved streamline analysis and fault visualisation.

Roxar Tempest, which runs on Windows and Linux and operates alongside Emerson’s reservoir characterisation and modelling solution Roxar RMS, is an integrated software suite that provides a wide range of reservoir engineering features and is used in hundreds of installations worldwide. All modules can be deployed together or separately within 3rd party simulation workflows. For more information on Tempest 8.2 visit www.emerson.com/ReservoirEngineering

*Nexus is a mark of Landmark (Halliburton)

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.