In the solvent extraction (SX) process, there is a continuous flow of leachate from leach pads to the SX plant. Isolation valves are installed on these lines to isolate the leaching solution, raffinate, and/or pregnant solution for maintenance purposes. Valves must resist the corrosive media and perform on demand with zero leakage isolation to secure the safety of personnel and the environment.
The following products are capable of providing zero leakage shutoff of leachate lines. These valves are engineered for long lasting performance in corrosive environments such as leach pads.
Based on many plant visits and discussions with Emerson customers, I have concluded that handling slurries is one of the biggest problems for operators and reliability teams. The most frequently mentioned issues are clogging and erosion, which certainly take their toll, but there is also a more subtle challenge related to measuring flow. Why slurries …
meer lezenEn este episodio los expertos en instrumentación industrial, Jorge Espinoza y Martín López nos comparten sobre las tecnologías de medición y monitoreo para variables críticas en la industria minera. Exponen sobre los más recientes avances en medición para incrementar la seguridad, la eficiencia y la rentabilidad de los procesos mineros. Te invitamos a ver o …
meer lezenEmerson’s Mathias Gehl, from the recently acquired Flexim organization presented Water Management Compliance with FLEXIM Non-Intrusive Flow Measurement at the 2024 Emerson Exchange Conference in Düsseldorf, Germany.
meer lezen