Isolation Valves
Reliable valve solutions for the safe shut off and isolation of industrial processes.
An isolation valve stops the flow of gas, liquid, slurry or powder. These valves typically operate in the closed or fully open position to direct process media, protect in emergencies and facilitate safe maintenance. Isolation valves are also known as shut off valves, on-off valves or stop valves.
Lined isolation valves and sampling systems for safe, reliable use in highly corrosive media applications.
Over the past 20 years, more and more countries around the world are focused on combating fugitive emissions. There’s a way for manufacturers to do their part, says Jeff Roseneder, by taking a closer look at basic seal design in ball valves.
Selecting components that are inappropriate for their operating environment is a major cause of issues that can be extremely costly to rectify. As Olivier Beyerman, director sales and business development at Emerson explained during his presentation at Emerson Exchange EMEA 2024 in Düsseldorf, the right isolation valve design for deployment in renewable diesel production can …
meer lezenModern digital valve controllers with onboard valve monitoring and diagnostics reduce unplanned outages and increase profitability. End users choosing controllers should carefully evaluate the features offered to take advantage of the significant advancements seen in the last few decades.
meer lezenJean-Paul Boyer, Massimiliano Franco, Nagendra Maddula, and Eugenio Sudati recently published an article in LNG Industry magazine, “The Key to Valve Selection for Challenging LNG Applications”. It describes key design parameters for choosing the best valves for LNG terminal operations.
meer lezenIsolation Valve FAQs
An isolation valve stops the flow of gas, liquid, slurry or powder. These valves typically operate in the closed or fully open position to direct process media, protect in emergencies and facilitate safe maintenance. Although there are differences in intended use, isolation valves are also commonly known as shut off valves, on-off valves or stop valves.
Isolation valves are available in variety of designs including ball valves, butterfly valves, gate valves, globe valves, knife gate valves and triple offset valves. Each design type has its own advantages depending on the process conditions, system design or goals of the plant owner.
Isolation valves are installed in piping systems to isolate flow to ensure safe maintenance of process equipment including control valves, pumps and tanks. Isolation valves can also be used for on-off process control, to connect external equipment, facilitate testing and to shut down processes in an emergency.
Valves are the leading source of fugitive emissions in a typical process facility. Leakage can occur around the valve stem, body seals and end connections resulting in the unintended release of process media. It is therefore critical to carefully select low emission valve technology that features quarter turn action, a proven stem seal system, minimal body joints and where possible, welded end connections.