Retrofitting controls on Alstom GT13 combustion turbines with Ovation™ technology expected to boost reliability and provide flexibility to support future expansion at DK6 plant PITTSBURGH (November 6, 2017) — ENGIE has awarded Emerson a contract to replace legacy combustion turbine controls with
Ovation™ turbine control technology at its DK6 800-MW combined-cycle power plant in Dunkirk, France.
The Ovation controls will be installed at each unit during a 13-day outage – a compressed timeframe for a turbine controls replacement project. This marks the first time a vendor other than the turbine OEM has been selected to retrofit GT13 combustion turbine controls.
“We considered different suppliers, and ultimately chose Emerson because its Ovation system met our requirements for support and maintenance over the expected 20-year life of the plant,” said DK6 Plant Manager Bernard Rulmont.
Flexibility was another factor in ENGIE’s decision to select Emerson, according to Rulmont.
Ovation is an open system, which gives DK6 personnel the ability to modify applications or adapt the controls to accommodate future plant expansion, as well as new operation modes and fuels – all without the need for a costly service call.
“Emerson understands the impact efficient turbine control has on achieving optimal levels of reliability and availability,” said Bob Yeager, president, Power & Water, Emerson Automation Solutions. “Our Ovation technology uses the same hardware and software platform for turbine control as it uses for other plant controls, such as heat recovery steam generators, burner management systems, generator excitation and high-fidelity embedded simulation. This single platform architecture significantly reduces O&M automation-related expenses and simplifies lifecycle management and planning.”
The first retrofitted power block is expected to be back online in September 2018; the second in July 2019. Emerson’s comprehensive project scope includes dismantling the existing controls, engineering and installing the new controls, and assisting with commissioning and startup.
Medios de comunicación:
• Contactos: contactos de prensa para Emerson a nivel mundial
Recursos adicionales:
• Únase a la Comunidad Emerson Exchange 365
• Conéctese con la unidad de negocios de Emerson Automation Solutions a través de TwitterFacebookLinkedIn YouTube
Sobre Emerson
Emerson (EMR en la bolsa de Nueva York) es una empresa global de software y tecnología que ofrece soluciones innovadoras para las industrias esenciales del mundo. Emerson es un líder en automatización que ayuda a fabricantes de industrias discretas, híbridas y de procesos a reducir las emisiones y cumplir con sus objetivos de sostenibilidad por medio de su cartera de automatización sin igual, incluyendo su participación mayoritaria en AspenTech. Para obtener más información, visite Emerson.com.